xUnit file example
Here is an example of an xUnit file showing only the tags and attributes read by Polarion. There follows a screenshot of the result of importing the example file.
<?xml version="1.0" encoding="UTF-8"?>
<!-- This example shows only tags, attributes and content which is currently read by Polarion
See http://windyroad.org/dl/Open%20Source/JUnit.xsd -->
<testsuites>
<!--Name of the root tag does not matter, but it must not be same as the ones below -->
<testsuite timestamp="2011-10-17T23:05:06">
<!-- testsuite tags can be nested, timestamp is not required and format is "yyyy-MM-dd'T'HH:mm:ssZ" -->
<testsuite>
<testcase name="someMethod" classname="SomeClass" time="0.285"/>
<!-- test case id is "SomeClass.someMethod", time is not required and is in seconds -->
</testsuite>
<testcase name="otherMethod" classname="SomeClass" time="0.001">
<failure message="failure message" type="package.Exception">
<!-- message and type are not required, all text content is added to the created defect -->
Failure details
</failure>
</testcase>
<testcase name="otherMethod" classname="OtherClass" time="0.002">
<error message="error message" type="package.OtherException">
Error Details
</error>
</testcase>
</testsuite>
</testsuites>
See also Integrate external testing tools.