Overview of Test Parameters and Iterations
In manual testing, it is common for the testing steps of a test case to be executed multiple times with variations in the test procedure. For example, the same set of steps might be run on desktop and mobile operating systems, and/or with different browsers on the different operating platforms, or an electromechanical component might be tested with different input voltages. Polarion's Test Parameters (or "Parameterized Testing") feature can help make the test specification process efficient and flexible.
The discussion of this feature assumes you are already familiar with the information in Creating and Managing Test Runs.