About Test Runs
Test Runs log instances of the running or performance of a defined set of Test Cases. Test Runs may log results of manual tests or automated tests run as part of a build. Test Runs also contain information about the status of the Test Run, results of the instance of testing that the Test Run represents, the test environment, and the build tested.
An individual Test Run is based on a Test Run Template. Polarion products that support test management come with predefined templates which can be customized or used as the basis for custom Test Run Templates.