xUnitFileImport job parameters
This topic documents the parameters of the xUnitFileImport job, which enables importing results of externally executed tests into Polarion, and creating a new Test Run in the process.
Parameters are optional unless otherwise specified. Parameters for importing test results during Mavin builds are also documented, and an example of the job configuration is also provided.
Name | Description |
---|---|
path | Required. Path to xUnit file, or to a folder containing xUnit files. (All XML files are imported and then deleted.) |
project | Required. ID of the project in which the job will create test case and defect Work Items as output of the job. |
idPrefix | Prefix for the ID (composed of prefix+timestamp) of Test Run created as output of the job. |
userAccountVaultKey | Reference to user authentication key contained in the User Account Vault in Administration User Management User Account Vault |
maxCreatedDefects | The number of failed tests before a summary Defect type Work Item will be created instead of individual Defect items for every failed test. (The default is 20.) |
maxCreatedDefectsPercent | The percentage of tests that can fail before a summary Defect type Work Item will be created instead of individual Defect items for every failed test. (The default is 10%.) |
templateTestRunId | ID of the template Test Run on which the Test Run created by the job is based. The template Test Run must exist in the same project specified in project. |
templateTestCaseId | ID of template Test Case type Work Item used as basis for Test Case items created by the job. The template Test Case must exist in the same project specified in project. |
templateDefectId | ID of template Defect type Work Item used as basis for Defect items created by the job. The template Defect must exist in the same project specified in project. |
idRegex | Fills ID of the created Test Run with regex matching the xUnit file name. |
groupIdRegex | Fills group.id of the created Test Run with regex matching the xUnit filename. |
field[N] | Replace [N] with a number between 1 and 3. Specify up to three fields that can be additionally filled with regex matching xUnit file name. |
field[N]Regex | Replace [N] with a number between 1 and 3. When field[N] is specified, use this parameter to fill Test Run field[N] with a regex matching xUnit file name. |
See the Monitor Topic and Configuring the Scheduler for more information.
Parameters for import in Maven Builds
Test results may be imported to a created Test Run during Maven builds by configuration in .polarion/builder/build.properties.
The parameters are identical to the parameters for the xUnitFileImport job, except that all must be prefixed with polarion.build.xUnit.import.
Unlike the xUnitFileImport job, however, xUnit files are not deleted after import.
The following parameters must also be specified in the Maven build configuration.
Parameter | Description |
---|---|
polarion.build.xUnit.import.enabled | Set to true to enable import of test results during the Maven build process. |
polarion.build.xUnit.import.path=custom/path | When import is enabled, specified the relative path to artifactId\target\surefire-reports in the job's working directory. |
polarion.build.xUnit.import.singleTestRun | Set to true to import all xUnit files to a single Test Run. Set false to import different xUnit files to separate Test Runs. |
See also: Integrate external testing tools.