Configuring PostgreSQL database
This component must be installed and properly configured before you can start the Polarion server. The Windows installer attempts to install the software and configure it to run with Polarion, including some optimization for best performance. If for any reason the installer is unable to optimize PostgreSQL, you should do it manually.
How do I
Securing the Polarion activation applicationEnter an error reporting email