Adjust server memory allocation
The default installation uses 640 m (megabytes) as the maximum memory allocation settings. This is fine for evaluation purposes but should be increased in production installations to avoid running out of memory.
Tip:
Set the Xmx/Xms values to 50% of the server's total ram.
Open the [POLARION_HOME]/polarion.ini file in a text editor.
Adjust the following values to half of the server's total RAM:
-Xms650m
-Xmx650m
(Use MEGABYTES as the measure. For example, for 2 GB, specify –Xmx2000m.)
Save the changed file.
Reinstall the Windows Service.
C:\Polarion\polarion\service.bat -install
Make sure the Polarion server is not running
Run the following utility:
C:\Polarion\polarion\service.bat -install
Restart Polarion.