Create a new project
To be able to create new projects, you must be granted that permission by an administrator. There are two basic scenarios for creating a project:
Create a completely new project from a Project Template. This creates a new folder in the repository as the project root.
Mark an existing repository folder as a project. In this way you can begin managing existing sources and other content with Polarion. This option requires permission to access global Administration.
Create a new Project from a template
Procedures for this are covered in the topic Create a New Project From a Template.
If you are in Administration, open Repository, then in Navigation select Projects, and use the New Project button on the Projects page of Administration to launch the New Project dialog box. The rest of the process is the same as described in the User Guide.