Methods for Animating All Objects
The objects provide these methods to animate them:
closeImg, createIcon, delAniPoint, delAniPoints, deleteIcon, existsIcon, getAniPoints, getBoundingBox, getIconSize, getPixel, getRefPoint, inheritPosition, inheritSizeAndOrientation, linkAniPoint, mirrorX, mirrorY, moveAniPoint, openImg, putIconToClipboard, resetIcon, saveIconToFile, setAniPoint, setAniConveyor, setCurrIconFromClipboard, setIconFromFile, setIconSize, setPixel, setRefPoint, turnIcon, and unlinkAniPoint.
To view all of the methods and attributes of the material flow object, open the window Show Attributes and Methods. The figure below illustrates the information using the example of the object Source.
Select Show Attributes and Methods on the context menu of the Class Library to show the attributes and methods of the selected Class.
Press the F8 key or click Show Attributes and Methods on the Home ribbon tab of the Frame into which you inserted an instance to show the attributes and methods of the selected Instance.
Related Topic
Related Topics
closeImgcreateIcon
delAniPoint
delAniPoints
deleteIcon
existsIcon
getAniPoints
getBoundingBox
getIconSize
getPixel
getRefPoint
inheritPosition
inheritSizeAndOrientation
linkAniPoint
mirrorX (general description)
mirrorY (general description)
moveAniPoint
openImg
putIconToClipboard
resetIcon
saveIconToFile
setAniLine
setAniPoint
setCurrIconFromClipboard
setIconFromFile
setIconSize
setPixel
setRefPoint
turnIcon
unlinkAniPoint