Attributes for Animating All Objects
The objects provide these attributes for manipulating the icons of most objects:
CurrIcon, CurrIconNo, CurrIconTransparent, NumAnimationEvents, ObjectAngle, ObjectMirrored, RotateAroundRefPoint, StatusWithIcons, ZoomX, and ZoomY.
To view all of the methods and attributes of the material flow object, open the window Show Attributes and Methods. The figure below illustrates the information using the example of the object Source.
Select Show Attributes and Methods on the context menu of the Class Library to show the attributes and methods of the selected Class.
Press the F8 key or click Show Attributes and Methods on the Home ribbon tab of the Frame into which you inserted an instance to show the attributes and methods of the selected Instance.
To set the value of an attribute, you might, for example, type:
Station1.Pause := true |
To get the value of an attribute, you might, for example, type:
print Station1.Pause |
Related Topic