Modeling the Material Flow
Modeling in 2D introduces you to the most important tasks you will face when you create your simulation model in Plant Simulation 2D. If you start a new simulation project from scratch, and at one point in time or another, you might also have to create a corresponding 3D model at the same time or in the future, you have to keep a number of criteria in mind to facilitate this.
If you want to use display panels for example, you have to create a 2D Only model. This is described in detail under Selecting Settings in Plant Simulation.
We renamed the following objects in Plant Simulation 14.1 and 14.2:
Up to Version 14.0 | From Version 14.1 on |
---|---|
Assembly | AssemblyStation |
Line | Conveyor |
ParallelProc | ParallelStation |
SingleProc | Station |
Entity | Part |
Up to Version 14.1 | From Version 14.2 on |
---|---|
TableFile | DataTable |
CardFile | DataList |
StackFile | DataStack |
QueueFile | DataQueue |
As we created some of the models for the Online Help in previous versions, some of the screenshots still show the previous names of the objects.
Go to Creating a Simulation Model
Go to Update an Old Model to the Current Version
Go to Modeling the Flow of Materials, Basics
Go to Modeling the Flow of Materials, Advanced
Go to Simulating Free-Flowing Materials and Fluids
Go to Simulating the Accrued Costs of the Machines and Parts
Go to Simulating the Power Consumption in Your Facility
Go to Modeling Workers and the Jobs They Do
Go to Modeling a Shift System
Go to Modeling a Lockout Zone
Go to Assembling Parts with the AssemblyStation
Go to Removing Parts with the Dismantle Station
Go to Picking and Placing Parts with the Pick-And-Place Robot
Go to Conveying Parts Laterally with the Converter
Go to Changing the Conveying Direction with the AngularConverter
Go to Aligning and Shrink-Wrapping Parts with the Turnplate
Go to Moving Parts On with the Turntable
Go to Modeling a Kanban System
Go to Modeling Transport Systems
Go to Preparing Data for the Simulation with DataFit
Go to Executing Simulation Experiments
Go to Packing a Model and Sending it to Another User
Compare Modeling in the 3D
Compare Animating the Simulation Model and Viewing the Results