Animating the Simulation Model and Viewing the Results
Animating the simulation model and viewing the results provides information about these topics:
Note:
We renamed the following material flow objects in Plant Simulation 14.1:
Up to Version 14.0 | From Version 14.1 on |
---|---|
Assembly | AssemblyStation |
Line | Conveyor |
ParallelProc | ParallelStation |
SingleProc | Station |
Entity | Part |
We renamed the following list objects in Plant Simulation version 14.2.
Up to Version 14.1 | From Version 14.2 on |
---|---|
TableFile | DataTable |
CardFile | DataList |
StackFile | DataStack |
QueueFile | DataQueue |
As we created some of the models for the Online Help in previous versions, some of the screenshots still show the previous names of the objects.
Compare Modeling in 2D
Compare Modeling in 3D