BookPntHRelative
Syntax
<MU-Path>.BookPntHRelative:real |
The attribute BookPntHRelative sets the relative position of the booking point of the MU designated by <MU-Path> in the z-dimension. You can enter a value between 0 and 1.
Data Type of the Value You Can Assign
You can assign a value of data type real.
Example
.MUs.Transporter.Length := 4.5 -- meters |
Note:
A long MU may be located on several objects at the same time!
Related Topics
Related Topics
Attributes of All Mobile ObjectsAutomaticRouting (Part, Container)
BookPnt
BookPntLRelative
BookPntWRelative
ConveyingDirection
Coordinate3D (MUs)
CostsActive (MUs)
Destination (MU)
DestinationWasReached
DistributeCosts
Length (MU)
MaterialCostsPerPiece
MUHeight
MUHeightWithContent
MULength
MUWidth
Name (MUs)
ProdStatOn
ResStatOn (MU class)
RouteWeightingAttr (Part, Container)
Stopped (MUs)
XPos (MUs)
YPos (MUs)