X-dimension (Container)
Enter the dimension of the loading space of the Container along the x-axis into this text box. The loading capacity is the product of X-dimension times Y-dimension. The greatest allowed value is one million.
When you decrease the dimension of the Container, make sure that no MUs are located on the storage places that will be deleted by this action! Either delete these MUs or move them to another storage place on the smaller loading space.
For loaded Containers, Plant Simulation distributes the animation points, onto which it places loaded MUs, according to the dimension that you entered. If this dimension is too great to show the loaded MUs reasonably well, Plant Simulation does not show any MUs at all, but draws a pattern to signify that the object is not empty.
As long as the loading space is half empty, Plant Simulation shows a hatch pattern. If the loading space is more than half full, Plant Simulation shows a checker pattern.
Half empty loading space | More than half full loading space |
---|---|
Related Topics