Path (Source)
Syntax
<Path>.Path:string |
Depending on the settings of you entered for TimeOfGeneration and MuSelection, the attribute Path either sets the path to the delivery list, the sequence table, the frequency table, or the MU class.
Note:
The Source does not produce parts whose time of creation is in the future when you assign a delivery table during the simulation.
Data Type of the Value You Can Assign
You can assign a value of data type string or object.
Example
MySource.Path := "MyDeliveryTable" |
Related Topics