CreationTableActive
Syntax
<Path>.CreationTableActive:boolean |
The attribute CreationTableActive sets if Plant Simulation writes all events, for which the Source produced MUs during a simulation run, into a table (true) or not (false).
Note:
The Source records the creation events in addition to the resource statistics it collects in any case.
Data Type of the Value You Can Assign
You can assign a value of data type boolean.
Example
MySource.CreationTableActive := true |
Related Topics