StatRelativeOccupationIR (material flow objects)
Syntax
<Path>.StatRelativeOccupationIR → real |
The read-only attribute StatRelativeOccupationIR returns the relative, i.e., capacity-based, occupancy with interruptions, i.e., with pauses and failures, of the object designated by <Path>. The relative occupancy with interruptions is calculated from the relation of the sum of the dwelling times of the MUs and the product of statistics collection period and capacity. The return value 0 stands for 0 percent, the return value 1 stands for 100 percent.
Return Value
The return value has the data type real.
Compare the sample models: Click the Window ribbon tab, click Start Page > Getting Started > Example Models and click Small Examples. Then, select the respective Category, the Topic, and the Example in the dialog Examples Collection and click Open Model.
Example
print MyStation.StatRelativeOccupationIR |
Related Topics
Statistics report, Material Flow Properties of the stationary objects
Statistics report, Material Flow Properties of the mobile objects
Related Topics
Read-Only Attributes for Statistics of the Material Flow ObjectsStatBlockingCount
StatBlockingDelta
StatBlockingMu
StatBlockingPortion
StatBlockingTime
StatEmptyCount
StatEmptyDelta
StatEmptyMu
StatEmptyPortion
StatEmptyTime
StatFailCount
StatFailDelta
StatFailMu
StatFailPortion
StatFailTime
StatMaxNumMUs
StatMinNumMU (material flow objects)
StatNumIn (material flow objects)
StatNumOut (material flow objects)
StatPausingCount
StatPausingDelta
StatPausingMu
StatPausingPortion
StatPausingTime
StatPoweringUpDownCount
StatPoweringUpDownDelta
StatPoweringUpDownMu
StatPoweringUpDownPortion
StatPoweringUpDownTime
StatPredeposition
StatRelativeEmptyPortion
StatRelativeFullPortion
StatRelativeOccupation (material flow objects)
StatSetUpCount
StatSetUpDelta
StatSetUpMu
StatSetUpPortion
StatSetupTime
StatStoppedCount (material flow objects)
StatStoppedDelta (material flow objects)
StatStoppedMu (material flow objects)
StatStoppedPortion (material flow objects)
StatStoppedTime
StatUnplannedCount
StatUnplannedDelta
StatUnplannedTime
StatUnplannedMu
StatWaitingDelta
StatWaitingCount
StatWaitingMu
StatWaitingPartsPortion (material flow objects)
StatWaitingPortion
StatWaitingResCount (material flow objects)
StatWaitingResDelta (material flow objects)
StatWaitingResMu
StatUnplannedPortion
StatWaitingResPortion (material flow objects)
StatWaitingResTime ( (material flow objects)
StatWaitingSetUpExpBlockingPortion
StatWaitingSetUpExpTime
StatWaitingSetUpExpWorkingPortion
StatWaitingSetUpExpDelta
StatWorkingDelta
StatWorkingCount
StatWaitingSetUpExpCount
StatWorkingMu
StatWaitingTime
StatWaitingSetUpExpWaitingPortion
StatWaitingSetUpExpMu
StatWaitingSetUpExpPortion
StatWorkingPortion
StatWorkingTime