StatPausingPortion
Syntax
<Path>.StatPausingPortion → real |
The read-only attribute StatPausingPortion returns the portion of the statistics collection period during which the object was Paused.
Return Value
The return value has the data type real.
Example
print MyStation.StatPausingPortion |
Related Topics
Tab Statistics of the material flow objects
Statistics report, Paused Time
Tab Type Statistics of the Drain
Related Topics
Read-Only Attributes for Statistics of the Material Flow ObjectsStatBlockingCount
StatBlockingDelta
StatBlockingMu
StatBlockingPortion
StatBlockingTime
StatEmptyCount
StatEmptyDelta
StatEmptyMu
StatEmptyPortion
StatEmptyTime
StatFailCount
StatFailDelta
StatFailMu
StatFailPortion
StatFailTime
StatMaxNumMUs
StatMinNumMU (material flow objects)
StatNumIn (material flow objects)
StatNumOut (material flow objects)
StatPausingCount
StatPausingDelta
StatPausingMu
StatPausingTime
StatPoweringUpDownCount
StatPoweringUpDownDelta
StatPoweringUpDownMu
StatPoweringUpDownPortion
StatPoweringUpDownTime
StatPredeposition
StatRelativeEmptyPortion
StatRelativeFullPortion
StatRelativeOccupation (material flow objects)
StatRelativeOccupationIR (material flow objects)
StatSetUpCount
StatSetUpDelta
StatSetUpMu
StatSetUpPortion
StatSetupTime
StatStoppedCount (material flow objects)
StatStoppedDelta (material flow objects)
StatStoppedMu (material flow objects)
StatStoppedPortion (material flow objects)
StatStoppedTime
StatUnplannedCount
StatUnplannedDelta
StatUnplannedTime
StatUnplannedMu
StatWaitingDelta
StatWaitingCount
StatWaitingMu
StatWaitingPartsPortion (material flow objects)
StatWaitingPortion
StatWaitingResCount (material flow objects)
StatWaitingResDelta (material flow objects)
StatWaitingResMu
StatUnplannedPortion
StatWaitingResPortion (material flow objects)
StatWaitingResTime ( (material flow objects)
StatWaitingSetUpExpBlockingPortion
StatWaitingSetUpExpTime
StatWaitingSetUpExpWorkingPortion
StatWaitingSetUpExpDelta
StatWorkingDelta
StatWorkingCount
StatWaitingSetUpExpCount
StatWorkingMu
StatWaitingTime
StatWaitingSetUpExpWaitingPortion
StatWaitingSetUpExpMu
StatWaitingSetUpExpPortion
StatWorkingPortion
StatWorkingTime