Deceleration (Conveyor)
Syntax
<Path>.Deceleration:acceleration |
The attribute Deceleration sets the Deceleration with which the Conveyor decreases its speed. Enter any real number greater than or equal to 0.
You can only set the deceleration after you activate Acceleration/AccelerationEnabled.
Data Type of the Value You Can Assign
You can assign a value of data type acceleration.
Example
MyConveyor.Deceleration := 1 |
Related Topic
Related Topics
Attributes of the ConveyorAcceleration (Conveyor)
AccelerationEnabled (Conveyor)
Accumulating (Conveyor)
AutomaticStop (Conveyor)
Backwards (Conveyor)
Capacity (Conveyor)
CurrentSpeed (Conveyor)
Length (Conveyor)
MUDistance
MUDistanceType
Speed (Conveyor)
SpeedCtrl (Conveyor)
Time (Conveyor)
Width (Conveyor)