CurrentSpeed (Conveyor)
Syntax
<Path>.CurrentSpeed:speed |
The attribute CurrentSpeed sets the Current speed of the Conveyor in the forward direction (positive number) or in reverse (negative number). Enter any real number.
You can only set the current speed after you activate Acceleration/AccelerationEnabled.
Data Type of the Value You Can Assign
You can assign a value of data type speed.
Return Value
When you enter -1 for an infinite speed, the return value is inf.
Example
MyConveyor.CurrentSpeed := 2 |
Related Topic
Related Topics
Attributes of the ConveyorAcceleration (Conveyor)
AccelerationEnabled (Conveyor)
Accumulating (Conveyor)
AutomaticStop (Conveyor)
Backwards (Conveyor)
Capacity (Conveyor)
Deceleration (Conveyor)
Length (Conveyor)
MUDistance
MUDistanceType
Speed (Conveyor)
SpeedCtrl (Conveyor)
Time (Conveyor)
Width (Conveyor)