getRowNo
Syntax
<Path>.getRowNo(RowIndex:any) → integer |
The method getRowNo searches for the row which contains a user-defined row index of the DataTable designated by <Path>. It returns the row number. If the row index does not exist, Plant Simulation returns -1.
Note:
If the table contains a large number of entries, you might want to activate Fast index access.
Parameter
The parameter RowIndex of data type any designates the row index which Plant Simulation searches.
Note:
The method only works for simple data types, such as string, integer, etc.
Return Value
The return value has the data type integer.
Example
MyDataTable.getRowNo("article1234") |
Related Topics
Related Topics
Methods for Rows of the DataTableappendRow
cutRow (DataTable)
getAlignmentRow (DataTable)
getBackgroundColorRow (DataTable)
getEditorRightsRow (DataTable)
getFontColorRow (DataTable)
getFontSizeRow (DataTable)
getFormula
insertRow
isAlignmentRow (DataTable)
setAlignmentRow (DataTable)
setBackgroundColorRow (DataTable)
setEditorRightsRow (DataTable)
setFontColorRow (DataTable)
setFontSizeRow (DataTable)
setFormula