getColumnNo
Syntax
<Path>.getColumnNo(ColumnIndex:any) → integer |
The method getColumnNo searches for the column which contains a user-defined column index of the DataTable designated by <Path>. It returns the column number. If the column index does not exist, Plant Simulation returns -1.
Note:
If the table contains a large number of entries, you might want to activate Fast index access.
The method only works for simple data types, such as string, integer, etc.
Parameter
The parameter ColumnIndex of data type any designates the column index which Plant Simulation searches.
Return Value
The return value has the data type integer.
Example
var column : integer |
Related Topics
Related Topics
Methods for Columns of the DataTablecutColumn
getAlignmentColumn (DataTable)
getBackgroundColorColumn (DataTable)
getColumnWidth (DataTable)
getColumnYDim
getDataType
getEditorRightsColumn (DataTable)
getFontColorColumn (DataTable)
getFontSizeColumn (DataTable)
getFormatString (DataTable)
getVisibility (DataTable)
insertColumn
isAlignmentColumn (DataTable)
setAlignmentColumn (DataTable)
setBackgroundColorColumn (DataTable)
setColumnWidth (DataTable)
setCommonFormat
setDataType
setDataTypeDefault
setEditorRightsColumn (DataTable)
setFontColorColumn (DataTable)
setFontSizeColumn (DataTable)
setFormatString (DataTable)
setVisibility (DataTable)