Create and navigate a build plan process
Before you perform initial planning, the high-level build plan has to be defined. In the ship building industry, this is equivalent to creating the ship breakdown structure for each vessel.
The build plan creation can be divided into these tasks:
Create the manufacturing model
Before you begin work in Next Generation Planning, an administrator must use Teamcenter and Teamcenter scripts to set the effectivity, create the manufacturing model (also known as the build element root), and link a collaborative design to it.
You can View the effectivity, but only the administrator can set the effectivity.
Create build elements
To define and use a build plan architecture and high-level schedule plan per vessel to create build elements, the senior planner creates and changes the order of build elements.
Create activities
The senior planner creates and changes the order of activities.