Create build elements and activities
Navigate to or search for and open a build element.
The build element page is displayed.
On the build element page, click the Build Strategy tab.
Tip:The breadcrumbs represent the scope of your build planning strategy. If the and commands are not displayed, select a higher breadcrumb.
Select the build element under which you want to create a new build element or activity. If nothing is selected, the new object is created as a brother to the objects in the table instead of a child of the selected object.
You can drill down in the list to locate the parent object you want.
Click one of the following commands:
Create a build element
Create an activity
Tip:You can add build elements and activities to build elements at any level in the structure.
Type a name and optional description.
Click Create or Create & Add More to add additional build elements or activities.
The create dialogs can be configured by your administrator so that the required attribute groups are available as part of the create dialog box.
Tip:If your administrator has granted you permission, you can move build elements and activities in the structure.