Create operations in a product BOP
You can either create operations directly in the plant BOP or you can add operations from a functional plan (product BOP) to the plant BOP.
To add operations from the product BOP, perform these steps:
Search and open or navigate to a product BOP.
The process station page is displayed.
In the Structure section of the Product BOP page, select a functional group to be the parent of the operations you create.
In the Operations section of the Product BOP page, click Create Operation .
In the Create Operation dialog box, select an operation type.
Type a name in the Name box.
(Optional) Type additional information in the Description box.
Click Create.