Create operations
You can either create operations directly in the plant BOP or you can add operations from a functional plan (product BOP) to the plant BOP.
To create operations directly in the plant BOP, perform these steps:
Search and open or navigate to a process station.
The process station page is displayed.
Click the Planning tab.
Click Create Operation .
In the Create Operation dialog box, select an operation type.
Type a name in the Name box.
(Optional) Type additional information in the Description box.
Click Create.
(Optional) You can create station reports.