Create a process area, line, or station
During process area planning, you can create process areas, process lines, and process stations if they do not already exist in the plant bill of process (BOP).
Navigate to the plant BOP.
Click Create Process Area .
Type a station name.
Production Process Planning automatically fills in the ID and Revision fields.
(Optional) Type a description.
Click Create.
Next, create operations inside the station.
Note:
To remove a process area, line, or station, select the item in the Areas table and click Delete .