Buttons within the General Options toolbar act on the entire Save process, regardless of selection (or lack of selection). This toolbar uses toggle buttons pull-down lists when several values are available. Refer to the table below for specific descriptions.
Button | Name | Description |
---|---|---|
Create JT | Activate this button to create JT's for each document to be saved in Teamcenter. |
|
Compute Mass Properties | Activate this button to compute Mass Properties of each document to be saved in Teamcenter. | |
Compute Mass Properties for the Main Body | Activate this button to compute Mass Properties for the main body (only) of each document to be saved in Teamcenter. | |
Save Active Shapes | Activate to save the current Active Shape of any CATPart or CATProduct in Teamcenter. The CATPart/CATProduct will be loaded in the same state as previously saved. | |
Hide/Show | Activate this button to manage Hide/Show for each document to be saved in Teamcenter | |
Check-in After Save | Activate to check-in the entire assembly to Teamcenter at the end of the Save process. Only items that have been modified are checked-in. Use Check-in After Save to avoid manually checking in items when saving large assemblies. |
|
Force Save for Unmodified Files | Activate this option by changing the value of CATIA_saved_modified_file_option to false, or by manually activating the Force Save for Unmodified Files button. Once activated, a message displays in the status bar indicating that modified and unmodified files are saved. The Status column of the Save Manager is updated according to the following rules:
In the illustrations below, an assembly containing Item ID 014667 is CI and 014669 is RO. The Status column displays a Warning indicating those elements cannot be saved. As a result, the Final Save Panel indicates that Item IDs 014665 and 014666 have been successfully saved. When Force Save for Unmodified Files is deactivated, the message in the status bar indicates Ready and the usual checks are performed on the modified files. |
|
Destination Folder |
Browse panel: Use Create Folder to display the New Folder panel and create a new directory to save the item to: |