Perform the following steps to configure the catia2jt script for the Theorem translator.
1. Locate
the catia2jt.bat or catia2jt file in the following Integration
install directory:
%TCICV5_DIR%\bin\WIN32 or $TCICV5_DIR/bin/{Os}.
2. Ensure the correct translator path for TS_INST=C:\Translator_Path is included in catia2jt.bat or catia2jt.
3. Define CATIAV5_ENV and CATIAV5_DIRENV. For example, CATIAV5_ENV = Teamcenter_Integration_for_CATIAV5 and CATIAV5_DIRENV = C:\apps\catia\R19\CATEnv.
4. Ensure the correct V5_EXE/V4_EXE line is activated in the catia2jt.bat or catia2jt file (Siemens or Theorem).