.bmp Thumbnail Files
On the
Client Machine |
Installation
Topics: Installing Translation Services
|
A .bmp preview of an item, item revision and/or dataset can be displayed as a thumbnail. Thumbnails of a selected item, item revision and/or dataset display in the Summary tab within Teamcenter Navigator.
There are two ways to create thumbnail previews:
1. On the client machine (Windows only)
2. Using Dispatcher Services. Dispatcher Server must be installed on a Windows operating system.
The illustration below displays a .bmp preview of a selected item revision
containing a CATProduct dataset. The .bmp file is added as a Named Reference
under the dataset.
Thumbnails can only be created for files that have been imported. Thumbnails can be updated for non-modified documents by performing a force Save in the Save Manager.