Solid Edge Draft Type Library
TangencyTolerance Property
Solid Edge Draft Type Library > DrawingView Object : TangencyTolerance Property
Description
Gets or sets the tangency tolerance, in degrees. 0.0 means use the default; otherwise the tolerance in degrees is > 0.0 but <= 5.0
Property type
Read-write property
Syntax
Visual Basic
Public Property TangencyTolerance As Double
See Also

DrawingView Object  | DrawingView Members  | Solid Edge V17 - What's New