Solid Edge Draft Type Library
ShadingShowVisibleEdges Property
Solid Edge Draft Type Library > DrawingView Object : ShadingShowVisibleEdges Property
Description
Specifies whether visible edges are shown in the referenced drawing view.
Property type
Read-write property
Syntax
Visual Basic
Public Property ShadingShowVisibleEdges As Boolean
Remarks
If the view was not previously shaded, changing the value of this property causes the drawing view to go out of date. You must call the Update method for the DrawingView object for the change to be displayed.
See Also

DrawingView Object  | DrawingView Members