Solid Edge Draft Type Library
SendBackward Method
Solid Edge Draft Type Library > DrawingView Object : SendBackward Method
Description
Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it.
Syntax
Visual Basic
Public Sub SendBackward() 
Remarks
This command is useful when objects are hiding other objects that have a lower priority display but when you do not want to send the object all the way to the back of the priority list.
See Also

DrawingView Object  | DrawingView Members