Solid Edge Draft Type Library
SectionFullModel Property
Collapse All
Expand All
View with Navigation Tools
Solid Edge Draft Type Library
>
DrawingView Object
: SectionFullModel Property
Description
Gets or sets whether a section of section view should ignore the previous sections
Property type
Read-write property
Syntax
Visual Basic
Public Property SectionFullModel As Boolean
Remarks
Using "View.ForceUpdate" is mandatory after using this API to see the effect in draft file.
See Also
DrawingView Object
|
DrawingView Members