Specifies whether show/hide settings are applied to reference components, e.g. ref planes, when using a configuration on this drawing view.
Visual Basic |
---|
Public Property ReferenceComponentsByConfigurations As Boolean |
Imports System.IO Imports System.Runtime.InteropServices Module Example <STAThread()> _ Sub Main() Dim objApplication As SolidEdgeFramework.Application Dim objDraftDocument As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objDrawingViews As SolidEdgeDraft.DrawingViews Dim objDrawingView As SolidEdgeDraft.DrawingView Try OleMessageFilter.Register() objApplication = Marshal.GetActiveObject("SolidEdge.Application") objDraftDocument = objApplication.ActiveDocument objSheet = objDraftDocument.ActiveSheet objDrawingViews = objSheet.DrawingViews For Each objDrawingView In objDrawingViews If objDrawingView.ReferenceComponentsByConfigurations Then objDrawingView.ReferenceComponentsByConfigurations = False Else objDrawingView.ReferenceComponentsByConfigurations = True End If Next Catch ex As Exception Console.WriteLine(ex.Message) Finally OleMessageFilter.Revoke() End Try End Sub End Module
using System.IO; using System.Runtime.InteropServices; internal static class Example { [STAThread()] public static void Main() { SolidEdgeFramework.Application objApplication = null; SolidEdgeDraft.DraftDocument objDraftDocument = null; SolidEdgeDraft.Sheet objSheet = null; SolidEdgeDraft.DrawingViews objDrawingViews = null; // SolidEdgeDraft.DrawingView objDrawingView = null; try { OleMessageFilter.Register(); objApplication = (SolidEdgeFramework.Application)Marshal.GetActiveObject("SolidEdge.Application"); objDraftDocument = objApplication.ActiveDocument; objSheet = objDraftDocument.ActiveSheet; objDrawingViews = objSheet.DrawingViews; foreach (SolidEdgeDraft.DrawingView objDrawingView in objDrawingViews) { if (objDrawingView.ReferenceComponentsByConfigurations) { objDrawingView.ReferenceComponentsByConfigurations = false; } else { objDrawingView.ReferenceComponentsByConfigurations = true; } } } catch (Exception ex) { Console.WriteLine(ex.Message); } finally { OleMessageFilter.Revoke(); } } }