Solid Edge Draft Type Library
IsLayerHidden Method
Solid Edge Draft Type Library > DrawingView Object : IsLayerHidden Method
Specifies the layer for which you want to determine hidden status.
Description
Returns True if the specified layer is hidden.
Syntax
Visual Basic
Public Function IsLayerHidden( _
   ByVal LayerName As String _
) As Boolean
Parameters
LayerName
Specifies the layer for which you want to determine hidden status.
See Also

DrawingView Object  | DrawingView Members