Solid Edge Draft Type Library
IsBroken Property
Solid Edge Draft Type Library > DrawingView Object : IsBroken Property
Description
Specifies whether the referenced view is a broken view.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsBroken As Boolean
Remarks
An object is broken when there is no longer associativity with the parent (for example, when the parent is deleted).
See Also

DrawingView Object  | DrawingView Members  | Solid Edge V18 - What's New  | Solid Edge V17 SP4 - What's New  | Solid Edge V16 SP9 - What's New