Solid Edge Draft Type Library
HighlightDrawingViewMembers Property
Solid Edge Draft Type Library > DrawingView Object : HighlightDrawingViewMembers Property
Description
Returns the HighlightDrawingViewMembers which can be used to highlight members.
Property type
Read-only property
Syntax
Visual Basic
Public Property HighlightDrawingViewMembers As HighlightDrawingViewMembers
See Also

DrawingView Object  | DrawingView Members