Solid Edge Draft Type Library
DisplayBreakLinesInBrokenState Property
Solid Edge Draft Type Library > DrawingView Object : DisplayBreakLinesInBrokenState Property
Description
Specifies whether or not break lines are displayed when the drawing view is in the broken state.
Property type
Read-write property
Syntax
Visual Basic
Public Property DisplayBreakLinesInBrokenState As Boolean
See Also

DrawingView Object  | DrawingView Members  | Solid Edge ST4 - What's New