Solid Edge Draft Type Library
CroppedVHL Property
Solid Edge Draft Type Library > DrawingView Object : CroppedVHL Property
Description
Specifies whether to generate only edges inside or overlapping the cropping boundary of the drawing view.
Property type
Read-write property
Syntax
Visual Basic
Public Property CroppedVHL As Boolean
Remarks
Geometry created with the Draw In View command is not affected by this setting.
See Also

DrawingView Object  | DrawingView Members  | Solid Edge V18 - What's New