Solid Edge Draft Type Library
CroppedBoundaryStyle Property
Solid Edge Draft Type Library > DrawingView Object : CroppedBoundaryStyle Property
Description
Specifies the default style name for the drawing view's cropped boundary. The cropped boundary shows only the portion of the border that is over visible geometry.
Property type
Read-write property
Syntax
Visual Basic
Public Property CroppedBoundaryStyle As String
See Also

DrawingView Object  | DrawingView Members  | Solid Edge ST2 - What's New