Solid Edge Draft Type Library
BringForward Method
Solid Edge Draft Type Library > DrawingView Object : BringForward Method
Description
Changes the display order of the referenced object by moving it in front of the first object that obscures it.
Syntax
Visual Basic
Public Sub BringForward() 
Remarks
This command is useful when other objects that are filled hide an object and the user wants to remove the object from hiding while not bringing the object to the top of the priority list.
See Also

DrawingView Object  | DrawingView Members