Adds annotations to select set which are connected to drawing view.
Visual Basic |
---|
Public Sub AddConnectedAnnotationsToSelectSet() |
Imports System.Runtime.InteropServices Public Class AddConnectedAnnotationstoSelectSet Private Sub btnAddConnectedAnnotationstoSS_Click(sender As System.Object, e As System.EventArgs) Handles btnAddConnectedAnnotationstoSS.Click Dim objApplication As SolidEdgeFramework.Application = Nothing Dim ObjDraftDocument As SolidEdgeDraft.DraftDocument = Nothing Dim objSheet As SolidEdgeDraft.Sheet = Nothing Dim objDrawingViews As SolidEdgeDraft.DrawingViews = Nothing Dim objDrawingView As SolidEdgeDraft.DrawingView = Nothing Dim objType As Type = Nothing Dim selset As SolidEdgeFramework.SelectSet = Nothing Dim i As Integer Try objApplication = Marshal.GetActiveObject("SolidEdge.Application") If objApplication Is Nothing Then ' Get the type from the Solid Edge ProgID objType = Type.GetTypeFromProgID("SolidEdge.Application") ' Start Solid Edge objApplication = Activator.CreateInstance(objType) ' Make Solid Edge visible objApplication.Visible = True End If ObjDraftDocument = objApplication.ActiveDocument 'getting the Active Sheet object objSheet = ObjDraftDocument.ActiveSheet objDrawingViews = objSheet.DrawingViews objDrawingView = objDrawingViews(0) 'Add dimensions to select set which are connected to Drawing View. objDrawingView.AddConnectedAnnotationsToSelectSet() selset = ObjDraftDocument.SelectSet i = selset.Count MsgBox(i.ToString) Catch ex As Exception MsgBox(ex.ToString) End Try End Sub End Class
using System.Windows.Forms; using System.Runtime.InteropServices; public class AddConnectedAnnotationstoSelectSet { private void btnAddConnectedAnnotationstoSS_Click(object sender, System.EventArgs e) { SolidEdgeFramework.Application objApplication = null; SolidEdgeDraft.DraftDocument ObjDraftDocument = null; SolidEdgeDraft.Sheet objSheet = null; SolidEdgeDraft.DrawingViews objDrawingViews = null; SolidEdgeDraft.DrawingView objDrawingView = null; Type objType = null; SolidEdgeFramework.SelectSet selset = null; int i = 0; try { objApplication = (SolidEdgeFramework.Application)Marshal.GetActiveObject("SolidEdge.Application"); if (objApplication == null) { // Get the type from the Solid Edge ProgID objType = Type.GetTypeFromProgID("SolidEdge.Application"); // Start Solid Edge objApplication = Activator.CreateInstance(objType); // Make Solid Edge visible objApplication.Visible = true; } ObjDraftDocument = objApplication.ActiveDocument; //getting the Active Sheet object objSheet = ObjDraftDocument.ActiveSheet; objDrawingViews = objSheet.DrawingViews; objDrawingView = objDrawingViews(0); //Add dimensions to select set which are connected to Drawing View. objDrawingView.AddConnectedAnnotationsToSelectSet(); selset = ObjDraftDocument.SelectSet; i = selset.Count; MessageBox.Show(i.ToString()); } catch (Exception ex) { MessageBox.Show(ex.ToString()); } } public AddConnectedAnnotationstoSelectSet() { SubscribeToEvents(); } private bool EventsSubscribed = false; private void SubscribeToEvents() { if (EventsSubscribed) return; else EventsSubscribed = true; btnAddConnectedAnnotationstoSS.Click += btnAddConnectedAnnotationstoSS_Click; } }