Solid Edge Draft Type Library
EditProperties Method
Solid Edge Draft Type Library > DraftDocument Object : EditProperties Method
Description
Displays the EditProperties dialog box to allow the user to interactively set and view various properties of the referenced document object.
Syntax
Visual Basic
Public Sub EditProperties() 
Remarks
These properties include general file properties, summary information, file attributes, units of measure, project information, and statistics such as the last time the file was saved, the last time the file was printed, and so forth.
See Also

DraftDocument Object  | DraftDocument Members