Solid Edge Draft Type Library
CreatedVersion Property
Collapse All
Expand All
View with Navigation Tools
Solid Edge Draft Type Library
>
DraftDocument Object
: CreatedVersion Property
Description
Returns the version of Solid Edge that was used to create the referenced document.
Property type
Read-only property
Syntax
Visual Basic
Public Property CreatedVersion As String
Remarks
If the file has never been saved, reading the CreatedVersion property returns an error.
See Also
DraftDocument Object
|
DraftDocument Members