Solid Edge Draft Type Library
SheetWindow Object
Members 
Solid Edge Draft Type Library : SheetWindow Object
Description
A 2-D view type that displays sheets and has a tab user interface.
Object Model
SheetWindow ObjectSection ObjectApplication ObjectSectionSheets CollectionSheet ObjectApplication ObjectArcs2d CollectionAreaPropertiesCollection CollectionSheet ObjectBlockLabels CollectionBlockOccurrences CollectionBoundaries2d CollectionBSplineCurves2d CollectionCircles2d CollectionComplexStrings2d CollectionCurves2d CollectionDrawingObjects CollectionDrawingViews CollectionEllipses2d CollectionEllipticalArcs2d CollectionImages2d CollectionLayers CollectionLines2d CollectionLineStrings2d CollectionPoints2d CollectionRelations2d CollectionSection ObjectSectionBoundaries2d CollectionSheetSetup ObjectSelectSet CollectionTextProfiles CollectionApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectBiDMEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFeatureSelectedFromPFEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionBackDrop ObjectSelectedSheets CollectionSelectSet Collection
Remarks
When a SheetWindow object is accessed, it is usually as a superset object called a View. If the window type is SheetWindow, then the methods and properties of the SheetWindow object extend to any standard Window object methods or properties.
See Also

SheetWindow Members