Solid Edge Draft Type Library
Section Object
Members 
Solid Edge Draft Type Library : Section Object
Description
A partition in a document that contains a list of sheets that belong to the partition.
Object Model
Section ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectBiDMEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFeatureSelectedFromPFEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionSectionSheets Collection
Remarks
The Section object contains a list of sheets that belong to that partition. Itemizing sheets from the Document object accesses all sheets in all sections. Itemizing sheets from the Section object accesses only the sheets in that section. In some applications, it will not be apparent that sections exist from the user interface. In these cases, Sheets are inserted into a default section.
See Also

Section Members