Drawing view type used to get or set the style name to use when creating drawing views of the specified type.
Member | Value | Description |
---|---|---|
seDVStyleMapping_2DmodelViews | 1 | |
seDVStyleMapping_AuxiliaryViews | 3 | |
seDVStyleMapping_ConnectorView | 9 | |
seDVStyleMapping_CuttingPlane | 5 | |
seDVStyleMapping_DetailEnvelope | 7 | |
seDVStyleMapping_DetailViews | 4 | |
seDVStyleMapping_NailboardView | 8 | |
seDVStyleMapping_PrincipalAndPictorialViews | 0 | |
seDVStyleMapping_SectionViews | 2 | |
seDVStyleMapping_ViewingPlane | 6 |