Solid Edge Draft Type Library
DetailEnvelope Object
Members 
Solid Edge Draft Type Library : DetailEnvelope Object
Description
Provides methods and properties of a detail view envelope object.
Object Model
DetailEnvelope ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectBiDMEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFeatureSelectedFromPFEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionDrawingView ObjectApplication ObjectBreakLinePairs CollectionBrokenOutSectionProfiles CollectionCoordinateSystems2d CollectionDraftProfile ObjectCuttingPlanes CollectionDetailEnvelopes CollectionDVArcs2d CollectionDVBSplineCurves2d CollectionDVCircles2d CollectionDVEllipses2d CollectionDVEllipticalArcs2d CollectionDVLines2d CollectionDVLineStrings2d CollectionDVPoints2d CollectionModelMembers CollectionReference ObjectGraphicMembers CollectionHighlightDrawingViewMembers ObjectModelMembers CollectionDrawingView ObjectDraftProfile ObjectApplication ObjectArcs2d CollectionBSplineCurves2d CollectionCircles2d CollectionDimensions CollectionEllipses2d CollectionEllipticalArcs2d CollectionLines2d CollectionRelations2d CollectionDrawingView ObjectApplication ObjectBreakLinePairs CollectionBrokenOutSectionProfiles CollectionCoordinateSystems2d CollectionDraftProfile ObjectCuttingPlanes CollectionDetailEnvelopes CollectionDVArcs2d CollectionDVBSplineCurves2d CollectionDVCircles2d CollectionDVEllipses2d CollectionDVEllipticalArcs2d CollectionDVLines2d CollectionDVLineStrings2d CollectionDVPoints2d CollectionModelMembers CollectionReference ObjectGraphicMembers CollectionHighlightDrawingViewMembers ObjectModelMembers CollectionDrawingView Object
Remarks
These methods and properties provide information and controls for the display and characteristics (such as text color) of the detail view's caption; the detail envelope line type, line width, and diameter; and so forth. The DetailEnvelope methods and properties are extended to a DrawingView object (type igDetailView) through the DrawingView.Annotation property. A detail DrawingView object is created with the AddByDetailEnvelope method of the DrawingViews collection object.
See Also

DetailEnvelope Members