Opens a file in Revision Manager.
Visual Basic |
---|
Public Function OpenFileInDesignManager( _ ByVal FileName As String _ ) As Object |
Option Infer On Imports System Imports System.Runtime.InteropServices Namespace Examples Friend Class Program <STAThread> Shared Sub Main(ByVal args() As String) Dim application As DesignManager.Application = Nothing Dim document As DesignManager.Document = Nothing Try application = New DesignManager.Application() application.Visible = 1 document = CType(application.OpenFileInDesignManager("C:\Part1.par"), DesignManager.Document) Catch ex As System.Exception Console.WriteLine(ex) End Try End Sub End Class End Namespace
using System; using System.Runtime.InteropServices; namespace Examples { class Program { [STAThread] static void Main(string[] args) { DesignManager.Application application = null; DesignManager.Document document = null; try { application = new DesignManager.Application(); application.Visible = 1; document = (DesignManager.Document)application.OpenFileInDesignManager(@"C:\Part1.par"); } catch (System.Exception ex) { Console.WriteLine(ex); } } } }