This method gets the value of a specified global parameter for the referenced
Application.
Visual Basic |
---|
Public Function GetGlobalParameter( _ ByVal Parameter As ApplicationGlobalConstants, _ ByRef Value As Variant _ ) As Long |
Value | Description |
---|---|
seApplicationGlobalAdminFileLocation | |
seApplicationGlobalApplyStatusToLinks | |
seApplicationGlobalAvailableRootFolder | |
seApplicationGlobalBaselinedRootFolder | |
seApplicationGlobalCheckInOnClose | |
seApplicationGlobalExcludedCharactersFromRevision | |
seApplicationGlobalInReviewRootFolder | |
seApplicationGlobalInsightCacheLocation | |
seApplicationGlobalInsightFolderMappingFileLocation | |
seApplicationGlobalInWorkRootFolder | |
seApplicationGlobalLogFilesLocation | |
seApplicationGlobalLookAheadVersion | |
seApplicationGlobalMakeRevisionsObsolete | |
seApplicationGlobalMaximumCharactersInRevision | |
seApplicationGlobalObsoleteRootFolder | |
seApplicationGlobalOfflineMode | |
seApplicationGlobalReleasedRootFolder | |
seApplicationGlobalRevisionDelimiter | |
seApplicationGlobalSearchScope | |
seApplicationGlobalShowProcessedActions | |
seApplicationGlobalStartingRevisionValue | |
seApplicationGlobalTeamcenterFormula | |
seApplicationGlobalUpdateDraft | |
seApplicationGlobalUploadOnClose |
Option Infer On Imports System Imports System.Runtime.InteropServices Namespace Examples Friend Class Program <STAThread> Shared Sub Main(ByVal args() As String) Dim application As DesignManager.Application = Nothing Try application = New DesignManager.Application() Dim Parameter = DesignManager.ApplicationGlobalConstants.seApplicationGlobalInsightCacheLocation Dim Value As Object = Nothing application.GetGlobalParameter(Parameter, Value) Catch ex As System.Exception Console.WriteLine(ex) End Try End Sub End Class End Namespace
using System; using System.Runtime.InteropServices; namespace Examples { class Program { [STAThread] static void Main(string[] args) { DesignManager.Application application = null; try { application = new DesignManager.Application(); var Parameter = DesignManager.ApplicationGlobalConstants.seApplicationGlobalInsightCacheLocation; object Value = null; application.GetGlobalParameter(Parameter, ref Value); } catch (System.Exception ex) { Console.WriteLine(ex); } } } }